990-5992F-001

Connect the Power Cables

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the two indicated plates from the bottom of the UPS.

    Rear View 60-80 kVA 400 V UPS

    Rear View 100 kVA 400 V/50 kVA 208 V UPS

  3. In dual mains systems, remove the three single mains brackets.

    Rear View 60-80 kVA 400 V UPS

    Rear View 100 kVA 400 V/50 kVA 208 V UPS

  4. Route the power cables through the bottom of the UPS.
  5. Connect the PE cable to the PE terminal.

    Rear View 60-80 kVA 400 V UPS

    Rear View 100 kVA 400 V/50 kVA 208 V UPS

  6. Connect the input, output, and bypass (if applicable) cables.
  7. Connect the battery cables.
  8. Fasten the cables to the cable relief in the bottom of the UPS.
  9. Reinstall the two plates in the bottom of the UPS.
QR code for this page

Was this helpful?