990-91202A-001

Battery Circuit Breaker Kit E3SOPT008 Specifications

DANGER
hazard of electric shock, explosion, or arc flash
The battery circuit breaker kit (E3SOPT008) must only be used with Easy UPS 3S and Easy UPS 3S Pro.
Failure to follow these instructions will result in death or serious injury.
Battery circuit breaker LV438118+LV438135 or
LV438880
Maximum configuration 4 hour runtime
Battery type VRLA
Number of blocks 32–40
Maximum battery short-circuit level (kA) 10
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?