990-91202A-001

Installation Procedure

NOTE: The illustrations in this manual shows installation in a 700 mm empty battery cabinet. The battery circuit breaker kit can also be installed in a 1100 mm empty battery cabinet or in a grounded metal box.
NOTE: The distance between the battery bank and the UPS must not exceed 200 m. Contact Schneider Electric for installations with a longer distance.
  1. Mount the battery circuit breaker kit. Follow one of the procedures:
  2. Connect the Signal Cables for Easy UPS 3S or Connect the Signal Cables for Easy UPS 3S Pro.
  3. Connect the Power Cables.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?