990-91202A-001

Mount the Battery Circuit Breaker Kit in a Grounded Metal Box

CAUTION
risk of equipment damage
Mount the battery circuit breaker in a grounded metal box.
Failure to follow these instructions can result in injury or equipment damage.
  1. Measure and mark the holes for mounting the battery circuit breaker kit in the metal box.
  2. Drill holes in each of the marked locations.
  3. Mount the battery circuit breaker kit in the metal box.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?