990-91079H-001

Location of Breakers - 400 V Systems

Location of Breakers in 3:3 UPSs

Rear View of the 10–15 kVA UPS for External Batteries

Rear View of the 10–15 kVA UPS with Internal Batteries

Rear View of the 20 kVA UPS for External Batteries

Rear View of the 20 kVA UPS with Internal Batteries

Rear View of the 30 kVA UPS for External Batteries

Rear View of the 30 kVA UPS with Internal Batteries

Rear View of the 40 kVA UPS for External Batteries

Rear View of the 40 kVA UPS with Internal Batteries

Location of Breakers in 3:1 UPSs

Rear View of the 10–15 kVA UPS for External Batteries

Rear View of the 10–15 kVA UPS with Internal Batteries

Rear View of the 20 kVA UPS for External Batteries

Rear View of the 20 kVA UPS with Internal Batteries

Rear View of the 30 kVA UPS for External Batteries

Rear View of the 30 kVA UPS with Internal Batteries

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?