990-91079G-001

Transfer a Single UPS from Normal Mode to Static Bypass Mode

Note
Check that the bypass source is working normally before transferring to static bypass mode.
  1. On the display, select and then select Function > To bypass .

    The LEDs on the user interface show as follows:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?