0000509775_02_en

Additional Placement Information for Batteries with Vents

If placed on top of batteries with vents: Make sure the distance (A) between the vent and the module is at least 10 cm (4 inches).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.