0000509775_02_en

Attach BC4Bxx Measuring Cable for 1.2–2 V Batteries with 2 Poles

  • (A) Pole screw
  • (B) Safety washer
  • (C) Washer
  • (D) Measuring cable
  • (E) Battery connector
  • (F) Battery pole
IMPORTANT: Attach the cable as close as possible to the battery poles, but above the battery connectors.

To attach the BC4Cxx measuring cable to the battery:

  1. Connect the red cables to the positive battery pole.
  2. Connect the black cables to the negative battery pole.
  3. Tighten the pole bolts with the torque value recommended by the battery manufacturer.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.