0000509775_02_en

Attach BC4Bxx Measuring Cable for 1.2–2 V Batteries with 4 or More Poles

  • (A) Pole screw
  • (B) Safety washer
  • (C) Washer
  • (D) Measuring cable
  • (E) Battery connector
  • (F) Battery pole
IMPORTANT: Attach the cable as close as possible to the battery poles, but above the battery connectors.
NOTE: If the battery has 4 poles connect the cable to all poles. If the battery has more than 4 poles it is sufficient to connect the measuring cable to only 4 poles. Use the same poles at each battery.

To attach the BC4Cxx measuring cable to the battery:

  1. Connect the red cables to the positive battery poles.
  2. Connect the black cables to the negative battery poles.
  3. Tighten the pole bolts with the torque value recommended by the battery manufacturer.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?