0000509775_02_en

BACS Bus Communication Cable Technical Data and Parts

Contacts Twisted pair RJ10
Certifications UL, CSA and CE

BACS Bus Communication Cable Parts

Part Number Part Name Length
0W49701 BACS COMM. BUS CABLE RJ10 0.25M 0.25 m (0.82 ft)
0W49702 BACS COMM. BUS CABLE RJ10 0.4M 0.4 m (1.3 ft)
0W49703 BACS COMM. BUS CABLE RJ10 0.7M 0.7 m (2.3 ft)
0W49704 BACS COMM. BUS CABLE RJ10 1M 1 m (3.3 ft)
0W49705 BACS COMM. BUS CABLE RJ10 1.5M 1.5 m (4.9 ft)
0W49706 BACS COMM. BUS CABLE RJ10 3M 3 m (9.8 ft)
0W49707 BACS COMM. BUS CABLE RJ10 5M 5 m (16 ft)
0W49708 BACS COMM. BUS CABLE RJ10 10M 10 m (32.8 ft)
0W49709 BACS COMM. BUS CABLE RJ10 20M 20 m (65.6 ft)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?