0000509775_02_en

Install Bus Interface (GX_R_AUX)

The GX_R_AUX is connected to the BACS bus with a BACS bus cable. It can be connected at various locations of the BACS bus that uses the COM3 port on the webmanager, for example, to a current sensor, a splitting box, repeater or a module.

If multiple GX_R_AUX devices are used, configure a unique address with the DIP switches on each GX_R_AUX device connected to the same webmanager.

NOTE: The maximum bus cable length depends where it is connected. For more information see Bus Cable Length and Wiring Details.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?