DOCA0248EN-11

General Features

The following table presents the availability of general features on Panel Server Advanced in firmware version 001.009.000.

Available

Not available

General features

Availability

Functionality

Separated network topology

Switched network topology

Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system)

Ability to disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) by using Panel Server webpages

Wi-Fi

2.4 GHz

5 GHz

External Wi-Fi antenna (reference: PASA-ANT1)

IEEE 802.15.4 communication

Wireless device

Maximum concurrent number of devices

PowerTag Energy sensors

85

PowerLogic Tag energy sensors

85

Acti9 Active devices

85

Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

85

Wireless CO2 sensors

85

Wireless temperature and humidity sensors

85

PowerTag A devices

85

PowerTag Ambient sensors

85

Easergy TH110/CL110 environmental sensors

85

PowerLogic HeatTag sensors

15

PowerTag Control devices

10

PowerLogic PD100 devices

15

Constraints within a mixed configuration:

  • Any combination of wireless devices listed in the table above must not exceed 40 devices.

  • The total number of PowerTag Control, PowerLogic HeatTag, and PowerLogic PD100 should not exceed 20 devices.

Modbus TCP/IP communication

128 Modbus TCP/IP devices maximum including devices physically connected to the Panel Server and virtual devices (that is, IEEE 802.15.4 devices connected to a child Panel Server gateway)

NOTE: The Panel Server supports 64 simultaneous Modbus TCP/IP client connections (for example, SCADA system).

Modbus SL communication

32 Modbus SL devices maximum

Human Machine Interface (HMI)

FDM128 Ethernet display

Configuration

User management by single user account

User management by multiple users with Role-Based Access Control (RBAC)

Alarms

  • In general, publication of alarms supported by the end devices.

  • Publication of alarms related to the following:

    • Communication issue between a device and Panel Server when available from the end devices

    • Alarm associated to ERMS on circuit breaker

    • The three levels of alarms from HeatTag sensors

    • Alarms associated to Breaker I/O device connected downstream to an I/O Smart Link gateway

    • Communication loss alarm for wireless device connected downstream to a child gateway.

Protocols

Modbus TCP/IP server

Modbus TCP/IP client

DHCP client

DHCP server

DPWS server

HTTPS

SFTP client

Data export

Panel Server webpages for publication on SFTP server

Publication on Schneider Electric cloud by using Panel Server webpages

CSV export on PC by using Panel Server webpages

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?