Commissioning and Monitoring Features
The following table presents the availability of commissioning and monitoring features on Panel Server Advanced in firmware version 001.010.000.
Commissioning and monitoring features |
Availability |
|
---|---|---|
Modbus serial communication |
Commissioning of feature to use the Modbus serial port in reverse mode by using Panel Server webpages |
|
Digital inputs (PAS800L) |
Commissioning by using EcoStruxure Power Commission software |
|
Commissioning by using Panel Server webpages |
||
Monitoring by using EcoStruxure Power Commission software |
||
Monitoring by using Panel Server webpages |
||
Status assignment from a list of predefined values for each generic input/output in the IO status setting by using EcoStruxure Power Commission software or Panel Server webpages |
||
Firmware update |
Applied to one Panel Server gateway by using EcoStruxure Power Commission software |
|
Applied to one Panel Server gateway by using Panel Server webpages |
||
Applied to several Panel Server gateways by using EcoStruxure Power Commission software |
||
Applied to several Panel Server gateways by using Panel Server webpages |
||
Backup restore |
Backup restore on a Panel Server of the same model by using EcoStruxure Power Commission software |
|
Backup restore on a Panel Server of the same model by using Panel Server webpages |
||
Configuration |
Configuration by using EcoStruxure Power Commission software |
|
Ethernet configuration for upstream communication by using Panel Server webpages |
||
Modbus configuration of Modbus TCP/IP and Modbus serial devices by using Panel Server webpages |
||
Selective pairing of wireless devices by using EcoStruxure Power Commission software |
||
Selective pairing of wireless devices by using Panel Server webpages |
||
Disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) in the Panel Server by using Panel Server webpages |
||
Monitoring |
Display of data of I/O Smart Link devices by using Panel Server webpages |
|
Display of data of Panel Server digital inputs by using Panel Server webpages |
||
Display of data of the supported devices (see commercial references in Supported Devices) by using Panel Server webpages |
||
Diagnostic by using Panel Server webpages |
||
Email notification |
Email notification of selected alarms by using Panel Server webpages |
|
Email notification of selected alarms by using EcoStruxure Power Commission software |
||
Data logging |
Access to 3-year data logger with predefined data sampling that can be configured by using Panel Server webpages |
|
Access to 3-year data logger with predefined data sampling with EcoStruxure Power Commission software |