DOCA0248EN-11

New Features

  • Data publication through HTTPS, with public certificate authority.

  • Security improvement for Panel Server claiming from EcoStruxure Energy Hub: Claiming procedure uses device code in addition to serial number of Panel Server. The device code is available with the serial number:

    • By flashing the QR code on the front face of the Panel Server

    • on the Panel Server webpages with Panel Server identification data

  • For PowerTag C I/O devices, send a schedule for output control from cloud. Once received and running, the function allows the Panel Server to remotely execute scheduled control orders, even if the connection to cloud is interrupted.

  • Improvement in management of remote configurations sent from a cloud application: For invalid configurations, an error is logged in the auto-diagnostic file and feedback is sent to the cloud application to improve troubleshooting.

  • After publishing a topology to the Schneider Electric cloud and receiving the associated remote configuration, the Panel Server displays the following information at Settings > Data publication > Topology:

    • Last remote configuration status

    • Last successful remote configuration date

  • For PowerTag devices, addition of reset of energy counters from Energy widget in Monitoring & Control page, with confirmation popup message.

  • New measurements added for applicable wireless devices:

    • Active power demand

    • Peak active power demand with date and time of occurrence

    • Reset of peak active power demand

      • per device on the device page at Monitoring & Control

      • for all associated devices at Settings > Wireless devices > Measurements management

  • Demand calculation time interval can be set at Settings > Wireless devices > Measurements management

  • Addition of supported device Power meter iEM2455

  • Custom models improvement: Supports logic code SMOD10K for data measurement in custom device model created from EcoStruxure Power Commission software and imported into the Panel Server

  • Panel Server webpage user experience improvements

    • Energy units displayed more consistently in Trending page.

    • Selected filters in Trending page are maintained when changing screens or device selection.

    • The same color code is used for alarms across different webpages

    • In the Monitoring & Control page, only measurements relevant to the selected device are displayed in Advanced data tab, to improve readability

    • In the Maintenance page, the Panel Server serial number is displayed when Schneider Electric Customer Care Center is authorized to access the Panel Server remotely.

    • Triangular ‘No data’ icon replaced with standard warning icon.

  • Diagnostic logs improved for better debugging experience

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?