Device code

Panel Server unique identifier and the credentials used in the following cases:

  • Secure claiming of the Panel Server from a cloud application

  • As a password for first connection to Wi-Fi access point of the Panel Server.

The Panel Server device code should be treated as confidential information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?