Remote Control and Scheduling From Cloud

Presentation

WARNING
UNEXPECTED START OF OPERATION
Only allow remote and/or scheduled control of loads for non-critical electrical loads that can safely be left unattended.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Remote control allows you to manage non-critical electrical loads remotely or send commands when the EcoStruxure Panel Server is connected to the Schneider Electric cloud service.

The function is supported for the following devices:

  • PowerTag C IO devices

  • Exiway Link devices

Availability

This function is available on Panel Server Entry, Universal, and Advanced.

Setting the Parameters

The output remote control function is enabled and disabled in the EcoStruxure Panel Server webpages, at Settings > Data Publication.

  1. In Publication method, select Schneider cloud services.

  2. In Remote control, click the toggle switch to enable and schedule remote control of outputs.

  3. Save the settings.

  4. Read the safety message popup and click Confirm or Cancel.

Remote Control Orders to PowerTag C IO Devices

The function allows you to:

  • Remotely execute control orders on a device connected via a PowerTag C IO device configured as contactor with feedback loop mode or impulse relay mode, by using the a Schneider Electric cloud application. For more information, refer to Configuration of PowerTag Control Devices Through Webpages.

  • Send a control schedule when the EcoStruxure Panel Server is connected to the Schneider Electric cloud service. The schedule allows the Panel Server to remotely execute scheduled control orders, even if the connection to the cloud is interrupted.

    When a schedule is received and running, the following information is displayed on the webpages :

    • In the page header, Control scheduling is displayed to the right of Cloud service

    • At Settings > Data publication > Remote control, the toggle switch is green.

  • Send real-time status updates of the monitored device to the Schneider Electric cloud.

Sending Commands to Exiway Link Devices

You can send the following commands to Exiway Link devices from the Schneider Electric cloud:

  • Locate a device

  • Disable/Enable periodic test

  • Start functional test

  • Switch on/switch off light

  • Synchronize Exiway Link devices

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?