Data Publication

Presentation

Data publication allows you to publish sampled data from connected devices (Modbus, wireless or input/output) using one of the following methods:

  • Schneider Cloud services

  • SFTP

  • HTTPS

With Panel Server Advanced, you can also activate email notifications on active alarms.

NOTE: When Schneider Cloud services is activated, data publication on SFTP or HTTPS servers are no longer available.

Set up data sampling before activating data publication. Data sampled before activation of data publication is also published, with the following limits:

  • Panel Server Entry and Universal: up to one month of sampled data

  • Panel Server Advanced: up to three months of sampled data. All previously logged data is retained, up to a maximum of three years of data.

Publication Methods

You can select the method and activate data publication from Panel Server on the EcoStruxure Panel Server webpages, at Settings > Data publication > Publication method:

  • Select Schneider Cloud services to send the sampled data to the Schneider Electric cloud. See detailed topic.

  • Select SFTP to send the sampled data to an SFTP server. See detailed topic.

  • Select HTTPS to send the sampled data to an HTTPS server. See detailed topic.

  • Select Email service for alarms to send email notifications on active alarms (Panel Server Advanced). See detailed topic.

  • Select SFTP & Email for alarms to activate SFTP publication or to combine both services (Panel Server Advanced). See detailed topic.

  • Select HTTPS & Email for alarms to activate HTTPS publication or to combine both services (Panel Server Advanced). See detailed topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?