Data Sampling
Presentation
The data sampling function on Panel Server samples data from connected devices at a defined frequency for a defined set of measurements. The frequency and measurements depend on the configuration of the function, set either by a connected cloud application or manually in the Panel Server webpages.
For Panel Server Entry and Universal, the sampled data is pushed to a buffer before being published. The buffer stores data for up to one month and publishes to the cloud application when data publication is activated or when the connection is restored after an interruption.
For Panel Server Advanced, the data is logged in the Panel Server.
Availability
This function is available on Panel Server Entry, Universal, and Advanced.
Setting the Parameters
Activate data sampling on the EcoStruxure Panel Server webpages, at .
Data Sampling Configuration from Cloud Application
When a connection to a cloud application is enabled, data sampling is automatically activated and configured by the cloud system. The settings are not editable (read only) with Panel Server webpages.
Data measured on the connected devices is sampled and published to the cloud application.
Manual Data Sampling Configuration
Manual data sampling allows you to configure the measurements to be sampled for each device in the system:
-
Modbus devices
-
Wireless devices
-
Input/output devices
After the commissioning of all the devices connected to the Panel Server, the choice of measurements and sampling period can be set individually for each device in the webpage :
-
For each device, click the device name.
-
Click Data.
-
Select or deselect sampling for every measurement with the Sampling checkbox.
-
Select the sampling period for the measurement. Refer to Changing the Data Sampling Frequency, if relevant.
-
Click Save to apply changes.
IMPORTANT: Applying the changes may take up to a few minutes. during which the following pages and functions are not accessible:-
Home page dashboard (Advanced)
-
Trending - device and aggregated data views (Advanced)
-
Custom models - custom model updates
-
CSV export
-
Backup and restore
-
Data sampling
-
Measurement sampling
-
Calculation of Valid Configurations for Data Measurements
-
A maximum of 5,000 simultaneous individual data points from different devices whatever the type (wireless, Modbus-SL, or Modbus TCP/IP, input/output devices)
-
A maximum of 500 samples per minute
-
A maximum of 500 individual alarms for monitoring and sending email notifications (with a maximum of 300 of those from Modbus-SL devices)
NOTE: Any remote configuration that tries to enable more than these limits is rejected.
The following table shows examples of data sampling configurations and indicates if they are valid or not:
Number of devices (A) | Number of measurements (B) | Sampling period (min) (C) | Total number of simultaneous data points (A x B) | Samples per minute (A x B) / C | Number of alarms | Valid configuration |
---|---|---|---|---|---|---|
30 |
30 |
15 |
900 |
60 |
550 |
No - number of alarms > 500 |
30 |
170 |
15 |
5,100 |
340 |
90 |
No - total number of simultaneous data points > 5,000 |
30 |
30 |
1 |
900 |
900 |
90 |
No - samples per minute > 500 |
30 |
30 |
15 |
900 |
60 |
90 |
Yes:
|
The following data sampling information is displayed at
to provide assistance with sampling calculation:-
Data maintenance status
-
Number of sampled measurements
-
Maximum number of allowed sampled measurements
-
Number of samples per hour
-
Maximum number of allowed samples per hour
Changing the Data Sampling Frequency
For Panel Server Advanced, when the sampling period (frequency) is changed locally or by a remote configuration, historical logged data points are retained and migrated to comply with the new sampling period, with the following results:
-
Reducing the frequency (for example, changing the period from 5 minutes to 10 minutes): The data points relevant to the reduced frequency are retained. Intermediate data points are deleted.
NOTICE Hazard of loss of dataReducing the sampling frequency results in the permanent loss of intermediate historized data points.Perform a data log export before reducing the frequency to avoid losing data.Failure to follow these instructions can result in equipment damage.For more information about exporting data, refer to Exporting Data Locally.
-
Increasing the frequency (for example, changing the period from 10 minutes to 5 minutes): Data points for which no historical data exists are duplicated from existing historical data (data points on either side), which may create non-linear trends where linear trends are expected.
Data Sampling Activation and Flushing
The following table describes the settings.
Parameter | Description |
---|---|
Sampling activation |
Used to activate/deactivate data sampling by the Panel Server.
|
Flush data |
Used to delete all sampling data. To delete data:
|