DOCA0172EN-13

Overcurrent at Voltage Loss

This alarm indicates that an overcurrent occurred during the time of voltage loss. This alarm occurs only if the option is activated. The alarm is managed only if the nominal current or the breaker rating (Ir) of the associated protection device has been set.

NOTE: The RMS value of the current during the voltage loss is available in the Modbus table. For more details, refer to DOCA0241EN EcoStruxure Panel Server - Modbus File . These measurements help to diagnose the root cause of the overcurrent.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Make sure that the cause of the overcurrent is identified and is fixed before closing the circuit.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?