DOCA0172EN-11

Environmental Sensor Data Availability

Presentation

The data transmitted by the environmental sensors to the EcoStruxure Panel Server depends on the type of environmental sensors. The following table indicates which data is available in the EcoStruxure Panel Server according to the type of environmental sensors.

Device Commercial References

The device commercial references used for each type of environmental sensors are:

  • CL110 (Contact your Schneider Electric representative for information about commercial references.)

  • TH110 (Contact your local Schneider Electric representative for information about commercial references.)

  • TRH (SED-TRH-G-5045)

  • TRHC02 (SED-CO2-G-5045)

Other Measurements

Data

CL110 TH110 TRH TRHC02

Temperature

Ambient humidity

Ambient CO2 level

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?