DOCA0172EN-15

IP Network Services (DPWS)

Presentation

The EcoStruxure Panel Server supports Devices Profile for Web Services (DPWS) protocol for IP network discovery.

Availability

This function is available on Panel Server Entry, Universal, and Advanced.

Setting the Parameters

The IP network services are set on the EcoStruxure Panel Server webpages, at Settings > Network communication > DPWS.

DPWS can be enabled or disabled.

DPWS Settings

Parameter Description

DPWS Activation

Used to enable/disable the DPWS service (enabled by default).

Silent mode

Used to enable/disable the silent mode (disabled by default). In silent mode, DPWS only answers requests.

Discovery type

Used to set the IP discovery type:

  • IPv4

  • IPv6

  • IPv4 & IPv6 (default setting)

TCP listening port

Used to enter manually the port number (default setting: 5357).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?