Modbus TCP/IP Server
Presentation
Devices connected downstream from the Panel Server can be accessed from an upstream edge system through Modbus TCP/IP.Availability
This function is available on Panel Server Universal and Advanced.
Setting the Parameters
Modbus TCP/IP server function is set as follows:
-
With EcoStruxure Power Commission software
-
On the Panel Server webpages, at .
Modbus TCP Server Settings
The following table describes the settings and where they are available.
Parameter | Description | EPC software | Webpages |
---|---|---|---|
Message timeout (ms) |
In Modbus network configuration, you can set the message timeout period for the Modbus TCP server. Setting used to set the time-to-live of a Modbus request in the Panel Server. Any messages older than this setting will be dropped. Values from 1,000 to 320,000 ms (default setting: 6,000 ms) The value that you set for the Modbus TCP server must meet both following conditions:
|
– | ✔ |