DOCA0172EN-16

EcoStruxure Panel Server User Interface Layout

Overview

The illustration shows the Panel Server user interface layout.

  1. Header

  2. Main menus

  3. Sub menus

  4. Display zone

  5. Icon for contextual menu

Header

The header displays the following information at the top of every page.

  1. Services and associated status

  2. User name

  3. Drop-down list (Language, Change password, Logout)

Header part

Description

User name

The user name is SecurityAdmin, a user account with administrator rights such as reading and changing the product configuration, adding or removing wireless devices, accessing system logs.

Language

The webpage language is English (US) by default. Other languages are available in the list.

Change password

Click to change the user password (see password requirements).

Logout

Click to log out from the Panel Server session.
It is recommended that you log out from the Panel Server when it is not in use.
You are logged out automatically after a certain time of no activity.

Service names

Services are displayed depending on the Panel Server model:

  • SFTP

  • HTTPS

  • Data sampling

  • Cloud service

  • Control scheduling

  • Email service (Advanced model)

  • Data maintenance

Service status

The icon displays the service status:

  • Service activated and operative

  • Service activated but inoperative

  • (Cloud service only):

    • Initial configuration of the Panel Server is complete, however these additional actions are needed: publish the topology and associate the Panel Server on the cloud application side.

    • The remote configuration sent by the cloud application is invalid and is rejected by the Panel Server.An error is logged in the auto-diagnostic log file to assist with troubleshooting. Data publication does not start. If data publication is in progress, it stops. Feedback is sent to the cloud application that sent the remote configuration.

  • (All services): A restart was initiated. The icon will change to green after a successful publication cycle.

  • Data maintenance operation in progress. The service name and status icon will disappear when the data maintenance operation is completed.

Main Menus

Cards and Sub-menus

The cards and sub-menus display the sub-levels available under the selected main menu. Fields with a red star icon should be filled in to help ensure the proper behavior of the gateway and devices.

Display Zone

The display zone shows the selected card or sub-menu in detail with all related fields.

Icons

The context-specific function icons displayed depend on the selected menu.

Icon Action

Open the contextual menu.

Close the contextual menu.

In Settings pages, save the setting changes and apply them on the Panel Server. Can be used to update a consistent set of parameters through multiple webpages.

  • If a mandatory field is left blank, the field is highlighted in red.

  • If inappropriate characters are entered in a field, the field is highlighted in red.

In Settings pages, save the setting changes without applying the configuration on the Panel Server.

Contextual icon:

  • In Settings pages, cancel the setting changes to return to the last saved settings.

  • In Network communication pages, restore settings of the network communication configuration. Used to reapply the full list of settings previously saved.

Go to the maintenance page of the selected device.

Go to the settings page of the selected device.

Go to the real-time data page of the selected device.

Go to the data management page of the selected device.

Go to the trending page.

Go to the monitoring and control page of the selected device.

Delete a device. Confirm the removal in the pop-up message.

Monitoring and Control Icons

Icon Description

The device is connected.

The device is not connected.

Data measurement value is out-of-date or invalid.

Trending Icons (Home Page)

The trending icons are displayed on the Home page depending on consumption trends.

Icon Description

The consumption of the commodity (for example, electricity) or a selected usage (for example, lighting) is increasing.

The consumption of the commodity (for example, electricity) or a selected usage (for example, lighting) is decreasing.

 

No icon is displayed if the consumption rate is not changing.

Alarm Icons

Icon Description

High-severity alarm appearance.

High-severity alarm disappearance.

Medium-severity alarm appearance.

Medium-severity alarm disappearance.

Low-severity alarm appearance.

Low-severity alarm disappearance.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?