Hardware Description
Panel Server Entry
Front face |
Bottom |
Top |
|
For information about installation of Panel Server Entry, consult the instruction sheet available on the Schneider Electric website: NNZ76760. |
Panel Server Universal
Front face |
Bottom |
Rear |
|
Top |
For information about installation of Panel Server Universal, consult the relevant instruction sheet available on the Schneider Electric website: GDE74119 |
Panel Server Universal Wired by Design
Front face |
Bottom |
Rear |
|
Top |
For information about installation of Panel Server Universal Wired by Design, consult the instruction sheet available on the Schneider Electric website: PKR28607. |
Panel Server Advanced
Front face |
Bottom |
Rear |
|
Top |
For information about installation of Panel Server Advanced, consult the relevant instruction sheet available on the Schneider Electric website For information about installation of Panel Server Advanced, consult the instruction sheet available on the Schneider Electric website: JYT24469. @writer: uncomment following list and adjust
content above when HWV2 is available
|
Hardware Version
The new models of Panel Server, PAS600LWD and PAS600PWD are released with hardware version 002.000.000.
To identify your hardware version, check in one of the following ways:
-
The information printed on the top of the Panel Server:
-
Hardware version 001.000.000: MAC address and serial number
-
Hardware version 002.000.000: MAC address, serial number, and HW: V2.0
-
-
In the Panel Server webpages at either of the following paths:
-
Panel Server Status LED
Ethernet Status LEDs
Restart Button
To restart the Panel Server:
-
Press and hold the button for more than 10 seconds then release it.
Result: The status LED turns steady orange.
-
Wait for the Panel Server to restart completely:
-
The status LED remains steady orange while the Panel Server is rebooting.
-
The status LED turns steady green when the Panel Server is in normal operation.
-
QR Code
When the QR code on the front face of a Panel Server is scanned with a smartphone connected to the Internet, the Go2SE landing page is displayed.
The landing page displays:
-
Information about the Panel Server
-
A list of menus
Tamper Detection
A tamper-indicating label helps detect unauthorized physical access into the Panel Server. This label is light grey with Schneider Electric written in black.
The following figure illustrates the position of the tamper-indicating label (A) affixed on the right-hand side of the Panel Server:
Before installing, operating, servicing, or maintaining the EcoStruxure Panel Server, check the tamper-indicating label integrity.
External Wi-Fi Antenna (Optional)
The external Wi-Fi antenna is an option for
-
Panel Server Universal (except Wired by Design models)
-
Panel Server Advanced
Use the external Wi-Fi antenna in specific use cases such as when the Panel Server is installed in a switchboard with metallic partitions and door. The antenna improves the quality of radio frequency signal.
Connect the Wi-Fi antenna (reference PASA-ANT1) at the bottom of the Panel Server and install the antenna on the roof of the switchboard.
For information about installation of the external antenna, consult the instruction sheet available on the Schneider Electric website: NNZ58425.
For information about Wi-Fi communication in the Panel Server system, consult DOCA0289•• Wireless Communication Architectures With EcoStruxure Panel Server - Design Guide.
External IEEE 802.15.4 Antenna (Optional)
The external IEEE 802.15.4 antenna is an option for Panel Server Advanced.
Use the external IEEE 802.15.4 antenna in specific use cases such as when the Panel Server Advanced is installed in a switchboard with metallic partitions and door and some wireless devices are located in a different place. The antenna extends the wireless network outside the switchboard.
Connect the IEEE 802.15.4 antenna (reference PASA-ANT1) at the top of the Panel Server Advanced and install the antenna on the roof of the switchboard.
For information about installation of the external antenna, consult the instruction sheet available on the Schneider Electric website: NNZ58425.
For information about wireless communication in the Panel Server system, consult DOCA0289•• Wireless Communication Architectures With EcoStruxure Panel Server - Design Guide.