IEEE 802.15.4 Communication
Presentation
In an EcoStruxure system where IEEE 802.15.4 wireless devices are connected to a Panel Server, these wireless devices are required to withstand EMC levels as per IEEE 802.15.4 standard for proper device performance. For details about supported Schneider Electric IEEE 802.15.4 wireless devices, refer to the relevant Panel Server firmware release notes:
-
DOCA0249•• EcoStruxure Panel Server Entry - Firmware Release Notes
-
DOCA0178•• EcoStruxure Panel Server Universal - Firmware Release Notes
-
DOCA0248•• EcoStruxure Panel Server Advanced - Firmware Release Notes
DANGER |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Use IEEE 802.15.4 communication only with ComPacT, PowerPacT, MasterPacT MTZ, and other qualified
devices.
Failure to follow these instructions will result in death or serious injury.
|
IEEE 802.15.4 wireless communication devices provide a compact and high-density metering solution with numerous and accurate data for building systems. These wireless devices can send temperature, humidity, energy, power, current, voltage, and power factor to the Panel Server.
Wireless devices are connected downstream to the Panel Server.
The maximum number of wireless devices that can be connected to one Panel Server is detailed in the related topic.
The Panel Server Advanced can be connected to an external IEEE 802.15.4 antenna to extend the wireless network.
Availability
This function is available on Panel Server Entry, Universal (except Wired by Design models), and Advanced.
Setting the Parameters
IEEE 802.15.4 communication function is set as follows:-
With EcoStruxure Power Commission software
-
On the Panel Server webpages, at
Configuration Settings
WARNING |
---|
UNINTENDED EQUIPMENT OPERATION OR ALTERED FEATURE OF
PROTECTIVE DEVICES
When installing a Panel Server in a metallic enclosure, and connecting it to an external IEEE
802.15.4 antenna, do not install this antenna within the enclosure.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Correct operation of protective devices installed in a metallic enclosure can be altered by a high level of IEEE 802.15.4 network radio frequency transmission power.
The following table describes the settings and where they are available.
Parameter | Settings | Description | EPC software | Webpages |
---|---|---|---|---|
Wireless network settings | Wireless activation |
Used to enable/disable wireless emission of the Panel Server (disabled by default). |
✔ | ✔ |
Channel mode |
Used to specify how the IEEE 802.15.4 channel is selected:
|
✔ | ✔ | |
Channel |
Enter the channel number. |
✔ | ✔ | |
Antenna selection |
Used to select the type of IEEE 802.15.4 antenna used in the architecture:
|
✔ | ✔ | |
Output power |
Output power level cannot be changed when the internal antenna or both antennas (internal and external) are used. Output power can be set only when an external IEEE 802.15.4 antenna is connected to a Panel Server Advanced:
NOTE: When a Panel Server connected to an external IEEE 802.15.4 antenna is installed
in a metallic enclosure, check that the antenna is not installed within
the enclosure.
|
✔ | ✔ | |
Wireless communication |
Communication period for ambient sensors (s) |
The communication period defines the length of time (in seconds) each wireless device sends data to the Panel Server. This is only applicable to real-time data and not to alarms that are immediately notified in case of event.
NOTE: If the
communication period is reduced, it can potentially impact the stability
of the wireless network, and indicator of radio quality may be degraded.
As standard, the Panel Server has a defined default value for each family of wireless devices.
The communication period can be adapted as follows, if needed:
|
✔ | ✔ |
Communication period for control devices (s) |
||||
Communication period for energy related devices (s) |
||||
Network occupancy |
Indicates the network occupancy as a percentage. |
???
|
✔ | |
Wireless device management |
Remove all devices |
Used to remove all wireless devices connected to the Panel Server. |
✔ |
✔ |
Settings of Wireless Devices Discovery
The following table describes the settings and where they are available.
Parameter | Settings | Description | EPC software | Webpages |
---|---|---|---|---|
Discovery | Selective list |
Used to discover a selective list of wireless devices to be connected to the Panel Server. |
✔ |
✔ |
Discovery status |
Indicates the status of the device discovery on the wireless network:
|
– | ✔ | |
Discovered devices | – |
Identification of the discovered wireless devices with device type, name, and model. |
✔ |
✔ |