DOCA0184EN-01

Switch to the Electrical Diagram or Single Line Diagram of Other Panels of the Same Project

The list of the panels in the project is accessible from the electrical diagram and single line diagram page.

To switch to another panel in the project:

  • Click on the name of the panel which is currently displayed.

  • Click on the name of another panel in the list.

QR code for this page

Was this helpful?