DOCA0184EN-07

Information on the Panel

The following information is displayed on the right side of the screen:

  • The characteristics of the enclosure.

  • The empty space in the panel.

  • The buttons to change the displayed layers of the panel.

  • Modification of the enclosure dimensions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?