DOCA0106EN-13

User Interface Layout

Overview

This graphic shows the EIFE user interface layout.

A Banner

B Menu tabs

C Subtabs

D Action button

E Display zone

Banner

The banner displays the following information at the top of all the pages.

Generic Information

Description

Date and time

Current date and time in the format yyyy-mm-dd hh-mm-sec

User name checked

Name of the user who has logged in

Logout

To log out the EIFE session, click Logout or close your browser. It is recommended to log out from the EIFE session when it is not in use.

Main Tabs

The main tabs are:

  • Monitoring

  • Control

  • Diagnostics

  • Maintenance

  • Configuration & Settings

Subtabs

The subtabs display the submenus under the selected main tab.

Action Buttons

The action buttons correspond to the selected tab and it varies.

The following table describes the interface buttons:

Button

Action

Apply

Applies the changes.

Cancel

Cancels the modifications to return to the last saved settings.

Display Zone

The display zone shows the selected subtab in detail with all the related fields.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?