DOCA0106EN-11

Time Zone

Time Zone Configuration

Step

Action

1

From the EIFE menu bar, click Configuration & Settings .

2

From the Configuration & Settings menu, in the General submenu, click Time Zone .

3

In Time Zone Configuration webpage, select the time zone of your region from the Time Zone list.

4

Select the Enable check box if you have to set the daylight saving time.

5

Select the beginning and end time of daylight saving from the Daylight Saving Time begins and the Daylight Saving Time ends list.

6

Click Apply to save the settings.

NOTE: The settings of Time Zone is applicable only when Date and Time is in Automatic mode.
QR code for this page

Was this helpful?