DOCA0106EN-11

Webpage Access

Group Access

Group

Access

Administrator

Full access to all webpages.

NOTE: It is recommended to change the default administrator password for system security the first time you log in.

Guest

Read-only access to selected webpages.

User-defined groups

Choosing from the following options, the administrator assigns webpage access for each group. The access levels are as follows:

  • None : A group has no access to selected webpage

  • Read-Only : The password grants a group read-only access to the selected webpage

  • Full : A group has the same access as the administrator group to the selected webpage

NOTE:
  • The Webpage Access is available for the Administrator only.

  • The Administrator has full access to all the webpages.

QR code for this page

Was this helpful?