Access to EIFE Webpages
Supported Web Browsers
Browser |
Version with Windows XP |
Version with Windows Vista |
Version with Windows 7 and later |
---|---|---|---|
Microsoft Internet Explorer |
IE 9.0 |
IE 9.0 |
IE 10.0, IE11.0 |
Microsoft Edge |
– |
– |
81.0.416.58 and later |
Mozilla Firefox |
15.0 |
20.0 |
20.0, 45.0 |
Google Chrome |
24.0 and later |
24.0 and later |
24.0 and later |
First Access to the EIFE Webpages
The EIFE name must be configured during the first access to the EIFE webpages.
WARNING |
---|
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY,
AND CONFIDENTIALITY
Change default passwords at first use to help prevent
unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
When the EIFE interface is accessed for the first time with SecurityAdmin user name (Security Administrator role), the user will be asked to change the default password.
The procedure to access the EIFE webpages for the first time depends on the operating system of the computer:
-
Windows Vista, Windows 7 and later, or newer operating systems
-
Windows XP or older operating systems
First Access Through PC with Windows Vista or Windows 7 and Later
Step |
Action |
---|---|
1 |
Disconnect the PC from the local area network (LAN) and switch off Wi-Fi. |
2 |
Connect an Ethernet cable from the computer to the EIFE interface or to the Ethernet switch inside the panel. |
3 |
Open . |
4 |
Click EIFE appears in the list of devices. and theNOTE: If the
EIFE
name is not displayed in the list of devices in , check if the
PC and the
EIFE
interface are not connected through the
router.
|
5 |
Double-click the selected EIFE , the login page automatically opens in the browser. NOTE: Default browser must be Microsoft Internet Explorer or Microsoft
Edge.
|
6 |
Enter NOTE: The user name and password are case-sensitive.
|
7 |
To change the default password, select from the user name arrow on the header.The page is displayed. |
8 |
Enter , , , , and to change the default password. |
9 |
Select the language from the box and then click . |
10 |
To locate the EIFE -XXYYZZ, click on the header. The ULP LED of the selected EIFE -XXYYZZ blinks for 15 seconds (test mode). |
11 |
To name the EIFE , select the menu, go to submenu, enter the device name and click |
12 |
Write the EIFE name on a blank device name label and stick it on the existing one. |
-
XXYYZZ is the last 3 bytes of the MAC address in hexadecimal format.
-
Check the firewall settings if DPWS is not enabled.
First Access Through PC with Windows XP
Step |
Action |
---|---|
1 |
Disconnect the computer from the local area network (LAN) and switch off Wi-Fi. |
2 |
Connect an Ethernet cable from the computer to the EIFE interface. |
3 |
Start the web browser. NOTE: The computer automatically uses the default
IP address 169.254.#.# (#=0–255) and the default subnet mask
255.255.0.0.
|
4 |
In the address text box, enter Example: For an EIFE with MAC address 00-B0-D0-86-BB-F7 or 0-176-208-134-187-247 in decimal, enter 169.254.187.247 in the address text box. |
5 |
Press , the login page automatically opens in the browser. |
6 |
Enter NOTE: The user name and password are case-sensitive.
|
7 |
To change the default password, select from the user name arrow on the header.The page is displayed. |
8 |
Enter , , , , and to change the default password. |
9 |
Select the language from the box and then click . |
10 |
To locate the -XXYYZZ, click ULP LED of the selected -XXYYZZ blinks for 15 seconds. on the header. The |
11 |
To name the -XXYYZZ, select the menu and click submenu, and enter the device name and then click . |
12 |
Write the EIFE name on a blank device name label and stick it on the existing one. |
Access to Webpages
Follow the Network Discovery, Name Browsing, and IP Address Browsing process to access the webpages.
The webpage access depends on the IT infrastructure.
Network Discovery
Follow the below procedure to access the EIFE webpages once the EIFE name has been configured.
Step |
Action |
---|---|
1 |
Connect the EIFE interface or the Ethernet switch inside the panel to the local area network (LAN). |
2 |
Connect the computer to the local area network (LAN). |
3 |
Open . |
4 |
Click EIFE name is displayed in the list of devices. , theNOTE: If the
EIFE
name is not displayed in the list of devices in , check if the
PC and the
EIFE
interface are not connected through the
router.
|
5 |
Double-click the EIFE name which is written on the device label located on the front face of the selected EIFE interface, the login page automatically opens in the browser. NOTE: Default browser must be Microsoft Internet Explorer
or Microsoft Edge.
|
Name Browsing
DNS server is mandatory.
Step |
Action |
---|---|
1 |
Connect the EIFE interface or the Ethernet switch inside the panel to the local area network (LAN). |
2 |
Connect the computer to the local area network (LAN). |
3 |
Start the web browser. |
4 |
In the address text box, enter the EIFE name which is written on the device label located on the front face of the selected EIFE interface. |
5 |
Press , the login page automatically opens in the browser.NOTE: If the
EIFE
interface does not appear in the list of devices in , check if the
PC and the
EIFE
interface are not connected through the
router.
|
IP Address Browsing
IP static configuration has to be set.
Step |
Action |
---|---|
1 |
Connect the EIFE interface or the Ethernet switch inside the panel to the local area network (LAN). |
2 |
Connect the computer to the local area network (LAN). |
3 |
Start the web browser. |
4 |
In the address text box, enter IP address given by the IT administrator. |
5 |
Press , the login page automatically opens in the browser.NOTE: If the login page in the web browser does not open
or does not display correctly, check if
in Internet Explorer
is checked. |