User Interface Layout
Overview
This graphic shows the EIFE user interface layout.

A |
Header |
B |
Menu bar |
C |
Submenu bar |
D |
Webpages |
E |
Display zone |
F |
Action button |
Header
The header displays the following information at the top of all the pages.

A |
EIFE name |
B |
Intrusive command mode |
C |
Date and time |
D |
IP address |
E |
Device Location |
F |
My Profile Logout |
G |
User name |
Header Part |
Description |
---|---|
EIFE name |
Device name of the EIFE interface. |
Intrusive command mode Intrusive Command Mode |
|
Date and time |
Current date in yyyy-mm-dd format. Current time in hh-mm-sec format. |
IP address |
IPv4 address of the interface. |
Device Location |
Click to locate the selected interface in your equipment: |
My Profile |
Click to change your account password in the window. |
Logout |
Click to log out from the EIFE session, or close your browser. It is recommended to log out from the EIFE session when it is not in use. |
User name |
Name of the user who has logged in. |
Menu Bar
The main tabs in the menu bar are:
Submenu Bar
The subtabs in the submenu bar display the submenus under the selected main tab.
Webpages
The navigation menu under each subtab lists the webpages for the selected submenu.
Action Buttons
The action buttons correspond to the selected tab and it varies.
The following table describes the generic action buttons on Setting and Security webpages:
Button |
Action |
---|---|
|
Applies the setting changes. |
|
Cancels the setting modifications and returns to the last saved settings. |
For some settings, after clicking EIFE interface to apply the new settings:
, a pop-up message is displayed for confirmation to restart the-
Click
to restart and apply the setting changes. -
Click
to cancel the setting modifications and return to the last saved settings.
Display Zone
The display zone shows the selected subtab in detail with all the related fields.