DOCA0106EN-14

Date and Time

Description

The DATE & TIME page allows you to:

  • Manually set the date and time of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

  • Automatically synchronize the date and time of the MasterPacT MTZ drawout circuit breaker to the EIFE time.

The users with Installer or Engineer role can change the date and time settings.

Navigation to the Date and Time Page

To view the DATE & TIME page, click SETTINGS > GENERAL > DATE & TIME .

Date and Time Settings

Parameter

Description

Date and time setting mode

Allows you to select the date and time setting mode of the MasterPacT MTZ drawout circuit breaker and its IMU devices:

  • Check Manual (default setting) to set manually the date and time in the dedicated fields.

  • Check Network Synchronization via NTP to set automatically the date and time by an external time server (NTP server).

Date

Allows you to set the present date manually in the format yyyy-mm-dd.

Time

Allows you to set the present time manually in the format hh:mm:sec.

NTP Settings

Parameter

Description

NTP server setting mode

Allows you to select the NTP server setting mode:

  • Check Obtain Servers Automatically via DHCP/BOOTP (default setting) to set the NTP servers automatically.

  • Check Manual to set manually the NTP servers names or addresses.

Primary NTP server

Allows you to enter manually the primary NTP server address.

Secondary NTP server

Allows you to enter manually the secondary NTP server address.

NOTE:
  • When both the NTP servers are not reachable by EIFE interface and another IMU device is setting the date and time, the EIFE interface date and time setting mode falls back to Manual automatically.

  • When the time setting mode is set to Manual, Time Zone Offset is reset to 0.

  • IPv6 is not supported for NTP server address.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?