IP Network Services
Description
The
page allows you to set and activate the IP network services.The users with Security Administrator role can edit the IP network services parameters.
Navigation to the IP Network Services Page
To view the
page, click .IP Network Services Parameters
Parameter |
Description |
Value |
---|---|---|
|
Allows you to enable/disable the Modbus/TCP service. |
Default setting: Enabled |
|
Allows you to enable/disable the secure communication over TLS and then by RBAC mechanism between EPC software and EIFE interface. NOTE: It is recommented to set it as Enabled. Once the secure commissioning
is enabled, if EPC software is connected to EIFE interface, user must
start a new discovery of the EIFE interface with EPC software.
|
Default setting: Disabled |
Allows you to set the port number of the secure commissioning server. |
Setting range:1–65534 Default setting: 49152 |
|
|
Allows you to enable/disable the secure Modbus for machine-to-machine service. NOTE: Machine-to-Machine secure communication requires
components that connect to the EIFE interface to support the Secure
Modbus communication.
|
Default setting: Disabled |
Allows you to set the port number of the secure Modbus server. |
Setting range:1–65534 Default setting: 802 |
|
Allows you to set the number of sessions for the secure Modbus server. |
Setting range:1–8 Default setting: 2 |
|
|
Allows you to enable/disable the FTPS server. |
Default setting: FTPS server is disabled |
|
Allows you to enable/disable the discovery (DPWS) of the EIFE interface automatically. |
Default setting: Enabled |
|
Allows you to set the port number of the HTTP/Web server. |
Setting range:1–65534 Default setting: 80 |
|
Allows you to enable/disable the HTTPS service and to set the port number of the HTTPS server. NOTE: After disabling the HTTPS, you should clear the browser
cookies before authenticating it again.
|
Setting range:1–65534 Default setting: Enabled (value: 443) |