Showing 111 - 120 of 387 results

Page 12 of 39
  • Setting the detection sensitivity

    ELKO - SmartMove Multiwire Dimmer Push – Wiser Home Device user guide

    Setting the detection sensitivity Setting the detection sensitivity Setting the detection sensitivity You can set the sensitivity level of the sensor. On the Home screen, tap . Tap Devices Lights Motion Dimmer Motion Detection Sensitivity and select any one of the following options: Low: Detects
  • Setting the device location

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting up a schedule

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    Setting up a schedule Setting up a schedule Setting up a schedule The dimmer can be fully controlled by a schedule. Once the schedule is set, the dimmer operates at a given time. On the Home screen, tap . Go to Schedules > to create a schedule. Enter the name of the schedule (A). In the TYPE
  • Setting up a schedule

    ELKO - Power Tag Control – Wiser Home Device User Guide

    Setting up a schedule Setting up a schedule Setting up a schedule The control device can be fully controlled by a schedule. Once the schedule is set, the device operates at a given time. On the Home screen, tap Automations . Go to Schedules and tap to create a schedule. Enter the name of the
  • Setting the device location

    ELKO - SmartSensor Leakage Wireless – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting the device location

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting the device manually

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    Setting the device manually Setting the device manually Setting the device manually As a standalone thermostat, you can set the following settings and operating parameters. Refer the following topics for more information on these settings: Sensor type selection Floor calibration setting Max guard temp. setting Boost mode
  • Setting up a schedule

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The shutter can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time. The devices can be fully controlled by schedule
  • Setting the threshold temperature

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Setting the threshold temperature Setting the threshold temperature Setting the threshold temperature Using the Wiser Home app, you can define the inside and outside temperature of a room above which the shutters shall close. To set the threshold inside and outside temperature: In the Seasonal Comfort Mode set-up page, tap Temperature. Set the inside and outside desired temperatures and tap Set.
  • Setting up a schedule

    ELKO - SmartSocket Double 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
Page 12 of 39