Showing 121 - 130 of 272 results

Page 13 of 28
  • LED Indication

    ELKO - SmartDim Multiwire Universal LED Rotary – Wiser Home Device user guide

    LED Indication LED Indication LED Indication Pairing User Action LED Indication Status Press the push button 3 times. LED blinks amber per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning off. Resetting User Action LED Indication
  • Økemodus

    Elko Wiser Home – Brukerveiledning for systemet (Norge)

  • LED Indication

    ELKO - SmartDim Multiwire Universal LED Push – Wiser Home Device user guide

    LED Indication LED Indication LED Indication Pairing User Action LED Indication Status Press the push button 3 times LED blinks amber per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning off. Resetting User Action LED Indication
  • ELKO - SmartSensor PIR wireless Wiser Home Device user guide

    select any of the following options (C): – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to
  • Troubleshooting

    ELKO - SmartSwitch Push Wireless Plus – Wiser Home Device User Guide

    button 3 times, the device LED blinks red/green for 30 s. Pairing mode has changed to Bluetooth mode. Press the top-right push button on the device 3 times, hold it for 20 s until the LED blinks red, and the device reboots into the correct mode (Zigbee mode). Unable to configure a group, edit, or
  • LED Indication

    ELKO - SmartSocket Single 16 A – Wiser Home Device user guide

    LED Indication LED Indication LED Indication Pairing User Action LED Indication Status Press the push-button 3 times LED blinks amber per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning off. Resetting User Action LED Indication
  • Valg av driftsmodus

    ELKO - SmartSensor dør/vindu trådløs – Brukerveiledning for Wiser Home-enhet

  • Climate control

    Elko Wiser Home – System User Guide (Norway)

    system is in cooling mode in a non-cooling room: The Radiator Thermostat shall not perform a Boost and shall display the same status as in Device Lock mode. The Room thermostat shall wake up using any of the 3 keys (+, -, O), but subsequent button presses will not change the set point. Domestic
  • Troubleshooting

    ELKO - SmartRelay Puck 10AX – Wiser Home Device User Guide

    not able to connect with the Hub. After pressing 3 times, the device LED blinks green/red for 30 s. This does not apply to newer Zigbee ® model. Pairing mode has changed. Factory reset the device. After reset, press the Setup/Reset button or push button 4 times and then hold for 20 s, until the LED
  • LED indications

    ELKO Smart Tag – Wiser Home Device User Guide

    LED indications LED indications LED indications Behavior Communication indicator light SmartTag switched off. SmartTag is searching for a Hub in pairing mode. SmartTag is in identification mode. SmartTag is in network. Normal communication with the Hub. Occasional loss of communication. Loss of communication with the Hub. Internal error detected.
Page 13 of 28