Showing 171 - 180 of 272 results

Page 18 of 28
  • Setting the room temperature using the app

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature. Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.
  • Creating an automation

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    interconnected device. Test Alarm - When the device is in test mode. Hush Mode - When the device is in hush mode. Maximum 10 conditions can be added. To remove a condition, swipe it left and tap (D). To set a specific time for your automation, tap When > Add time and select any of the following (E
  • ELKO - Smart Plug 16 A

    of an automation Example of an automation In the example below, if away mode is enabled during Daytime, then Plug will turn off. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 elko.no/contact www.se.com Editing an automation Editing an automation Schneider
  • Adding a Device

    Elko Wiser Home – System User Guide (Norway)

    mode. The Wiser Home App will guide you through the pairing process. You can find detailed information about the pairing mode in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices. When the pairing is complete, you can give
  • Using the device

    ELKO - Schneider Charge – Wiser Home Device User Guide

    E, F, G, H, J. A Total cost of charging session. B Total time of charging in the session. C Total energy consumption in the session. D Control button (Start charging/Stop charging, Pause/Resume). E To select the charging mode. Refer to Charging Mode. F To see the 24 hr schedule based on the
  • Creating a moment

    ELKO - Smart Radiator Thermostat – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Creating a Moment

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    to set the condition. For example, select heating. Set the required temperature using the slider (D). If you move the slider to the bottom of the bar, Frost Protection mode is activated. In this mode, the system maintains the room temperature at 5 °C. When the desired condition is set, tap Set. Once
  • Wake up the Device

    ELKO - Wiser Room Thermostat – Wiser Home Device user guide

    Wake up the Device Wake up the Device Wake up the Device If there has been no interaction for 15 seconds, the Room Thermostat goes into Sleep Mode, and the display fades out. Wake up the Room Thermostat by tapping any button.
  • Creating a schedule

    ELKO - Schneider Charge – Wiser Home Device User Guide

    . Tap Charging Mode. If you have Schneider Charge installed with Wiser Hub you can also navigate the following path to create schedules: On the Home screen, tap . Tap Schedules > EV schedule. Proceed with step 3. On the EV Charging Mode page, select Customized Schedule. The Schneider Charge will
  • Setting the device manually

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    Setting the device manually Setting the device manually Setting the device manually As a standalone thermostat, you can set the following settings and operating parameters. Refer the following topics for more information on these settings: Sensor type selection Floor calibration setting Max guard temp. setting Boost mode
Page 18 of 28