Showing 191 - 200 of 272 results

Page 20 of 28
  • LED Indications in Quick Home Connect

    ELKO - SmartDim Multiwire Universal LED Push – Wiser Home Device user guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
  • Setting the threshold temperature

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Setting the threshold temperature Setting the threshold temperature Setting the threshold temperature Using the Wiser Home app, you can define the inside and outside temperature of a room above which the shutters shall close. To set the threshold inside and outside temperature: In the Seasonal Comfort Mode set-up page, tap Temperature. Set the inside and outside desired temperatures and tap Set.
  • Creating a Schedule/Event

    ELKO - Smart Radiator Thermostat – Wiser Home Device user guide

    schedule, the Frost Protection mode is activated when the schedule begins.In the frost protection mode, the system maintains the room temperature at 5 °C. Set time (for example 12:00). A maximum of 8 events can be created per day. You can tap to copy the schedule from one day to other days or copy the
  • Creating a moment

    ELKO - Wiser Underfloor Heating Connection Strip – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Resetting the device

    ELKO - SmartRelay Puck 10AX – Wiser Home Device User Guide

    Resetting the device Resetting the device Resetting the device Select any one of the options to reset the device to factory default mode: Short press the Setup/Reset button 3 times and then long press it once for 10 s using the screwdriver on the puck. Short press the push button 3 times and then long press it once for 10 s.
  • LED Indications in Quick Home Connect

    ELKO - SmartSwitch Push Wireless Plus – Wiser Home Device User Guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
  • LED Indications in Quick Home Connect

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
  • LED Indications in Quick Home Connect

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
  • Resetting the device manually

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    Resetting the device manually Resetting the device manually Resetting the device manually Short press (< 0,5 s) the Setup/Reset button 3 times and then long press the Setup/Reset button once for >10 s to reset the smoke alarm to factory default mode. All configuration data, user data and network data are deleted.
  • Troubleshooting

    ELKO - Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Troubleshooting Troubleshooting Troubleshooting Symptom Possible cause Solution The relay displays offline in the app or the LED flashing or solid red. Weak or no signal between the Wiser Hub and the relay. The relay is working in degraded mode. Check Hub is online. Check signal strength. The relay is flashing green. Emergency heat is active. Press the button to cancel the emergency heat function.
Page 20 of 28