Showing 21 - 30 of 272 results

Page 3 of 28
  • Creating an automation

    ELKO - Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away
  • Creating an automation

    ELKO - Wiser Room Thermostat – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away
  • Creating an automation

    ELKO - Smart Plug 16 A – Wiser Home Device User Guide

    conditions and select any of the following (C): Device status change: To select a device to enable automation. Away Mode: Enable / Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information refer to
  • Creating an Automation

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    : Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about , refer to the System User Guide. Tap Device status change > . Set the
  • Understanding Control Mode Priorities

    Elko Wiser Home – System User Guide (Norway)

    overriding the Wiser Home AI schedule. Scenario 2: You have a predefined schedule for your living room light to turn on every day at 6 PM and turn off at 10 PM. You have also set the living room light to turn Off when in away mode. At 7 PM, you leave home unexpectedly and activate Away Mode for an emergency. Response: The Away Mode overrides the predefined schedule and turns Off the living room light until the next trigger.
  • Creating an automation

    ELKO - Wiser Underfloor Heating Connection Strip – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about
  • Creating an automation

    ELKO - Motion Sensor Outdoor, 360 – Wiser Home Device user guide

    status change: To select a device to enable automation. Away Mode: To turn OFF the motion sensor and the device connected to it by enabling this mode. When the away mode is triggered, sensitivity of the motion sensor turns OFF. You can enable the motion sensor and the device connected to it by
  • Creating an automation

    ELKO - Schneider Charge – Wiser Home Device User Guide

    Add conditions (C) and select any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Energy Price changes (To define the energy price limit.) This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. Maximum
  • Creating an automation

    ELKO - SmartMove Multiwire Dimmer Push – Wiser Home Device user guide

    . Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User Guide. Tap Device status change > Motion Dimmer and select any of the following options: Dimmer On / Off: Select the dimmer
  • Creating an automation

    ELKO - SmartSensor Climate Wireless – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about
Page 3 of 28