Showing 21 - 30 of 86 results

Page 3 of 9
  • Setting the room temperature using the app

    ELKO - Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing. When you add it to your Favourites. To know more about Favourite, refer to the Managing Favourite topic in the respective System
  • Setting the room temperature using the app

    ELKO - Wiser Underfloor Heating Connection Strip – Wiser Home Device user guide

    on the Control tab, in the Heating section of the concerned room to adjust its temperature. When you add it to your Favourites. To know more about Favourite, refer to the Managing Favourite topic in the respective System User Guide. If you only have a single device in the Wiser System, the Control
  • Device control

    Elko Wiser Home – System User Guide (Norway)

    schedule or assign the device to an existing schedule. Refer to Schedule for detailed information. E Redirects you to Schedule details screen to modify your existing schedule. Refer to Editing a Schedule. F Add or remove the device from Favourite devices. Refer to Managing Favourites. G Navigates to the Device Details.
  • Managing the cable

    ELKO - Schneider Charge – Wiser Home Device User Guide

    Managing the cable Managing the cable Managing the cable Make sure that the charging connector and charging cable are securely stored between charging sessions. Wrap the charging cable around the charging station’s cable trough. If the Schneider Charge is installed outdoors, Remove the cap. If the Schneider Charge is installed indoors, protect the connector by covering it with the dust cap.
  • Managing Matter Connection

    Elko Wiser Home – System User Guide (Norway)

    Managing Matter Connection Managing Matter Connection Managing Matter Connection On the Home screen of the Wiser Home app, tap . Tap Account App and Connections Matter. Choose one of the following options: Manage your connections: Here you can see all Wiser Home system that are currently joined to
  • Climate control

    Elko Wiser Home – System User Guide (Norway)

    be available. H Add or remove the device from Favourite devices. Refer to Managing Favourites J Navigate to the Room Details of the room to which the climate control is assigned. Setting up a Climate Control While setting up your Climate Control, make sure to consider the following information
  • Managing shutter operation without temperature sensor

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Using the Wiser Home app, you can manage the shutter operation of a room where no temperature sensor is installed. To define the
  • Managing shutter operation without temperature sensor

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Using the Wiser Home app, you can manage the shutter operation of a room where no temperature sensor is installed. To define the
  • Using the device

    ELKO - SmartSensor Door/Win Wireless – Wiser Home Device user guide

    Using the device Using the device Using the device The Control Panel of the sensor allows you to view if the window/door is opened or closed. On the Control tab, tap All devices or a room tab where the sensor is located. On the sensor control panel page, you can see the following: Window/Door status (A) History (B) Device settings (C) Add to favourites (D)
  • Using the device

    ELKO - SmartSensor Leakage Wireless – Wiser Home Device user guide

    Using the device Using the device Using the device The Control Panel of the Sensor allows you to monitor the current status of water leakage detection. On the Control tab, tap All devices or a room tab where the sensor is located On the Sensor control panel page, you can see the following: Water leakage status (A) History (B) Device settings (C) Add to favourites (D)
Page 3 of 9