Showing 291 - 300 of 387 results

Page 30 of 39
  • Technical Data

    ELKO - Smart Radiator Thermostat – Wiser Home Device user guide

    Technical Data Technical Data Technical Data Power supply 2 x 1.5 V IEC LR6 (AA) alkaline batteries or 2 x HR6 NiMH batteries Without power supply: Connection data are retained Temperature setting range 5 °C - 30 °C Temperature resolution 0.5 °C Control accuracy < 0.8 °C at 4 °C/h Surface
  • Home Screen Settings

    Elko Wiser Home – System User Guide (Norway)

    Home Screen Settings Home Screen Settings Home Screen Settings The Wiser Home App offers options to customize the Home Screen. Find the Home Screen options in the Settings Menu. Setting ON OFF Start on Control Tab The App opens directly in the Control tab. The App will open on the Home Screen. Show
  • Amazon Alexa

    Elko Wiser Home – System User Guide (Norway)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • Checking the device history

    ELKO - SmartSensor Leakage Wireless – Wiser Home Device user guide

    lost, the leakage detected events will not appear in the history. On the Control tab, tap All devices or a room tab where the sensor is located. On the device control panel page, tap History. The history page displays all logged-in events, even if the sensor notification toggle switch is disabled. For more information about sensor notification toggle switch, refer to Setting device notification.
  • Enabling cooling input

    ELKO - Wiser Underfloor Heating Connection Strip – Wiser Home Device user guide

    Cooling Input toggle switch. If UFH channel is assigned to any of the following heating device, make sure in Room Setting Excluded From Cooling toggle switch is On. This can be useful if there are areas in a building that do not require cooling, such as storage rooms or unoccupied spaces. Smart ZB Thermostat 16 A
  • Using the device

    ELKO - SmartSwitch Push 10A – Wiser Home Device user guide

    Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. C Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. D Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.
  • Pairing the device with the Wiser Hub

    ELKO - Wiser Room Thermostat – Wiser Home Device user guide

    to update refer Setting Floor Sensor Location. Tap Submit to complete the pairing process. After you pair the device, a success screen appears with the following options: + Add New Device: Tap to continue pairing more devices. Start Using Your Device: Tap to start using the paired device. The success
  • Checking the device history

    ELKO - SmartSensor Door/Win Wireless – Wiser Home Device user guide

    , the window or door events will not appear in the history. On the Control tab, tap All devices or a room tab where the sensor is located. On the device control panel page, tap History. The history page displays all logged-in events, even if the sensor notification toggle switch is disabled. For more information about sensor notification toggle switch, refer to Setting device notification.
  • Relay Cycle Time

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    Relay Cycle Time Relay Cycle Time Relay Cycle Time In advanced settings, you can choose Relay Cycle Time (A). This setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle
  • Using the device

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    the sliding bar up/down to increase/ decrease the brightness. B Tap to manually turn the device ON/OFF. C Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Setting up a schedule topic. D Add to favourites Tap to add the device to the
Page 30 of 39