://download.schneider-electric.com/files?p_Doc_Ref=EKO025212n_HW Time setting Time setting: Adjusts the duration for which the sensor activates or triggers the connected load afterdetecting motion. NOTE: If you re-trigger the sensor, the timer will get reset. You can also change the status of the
the Wiser Hub ........................................................10Configuring the device ..............................................................................13 Setting the device location ...................................................................13User interface lock
device with the Wiser Hub ........................................................10Configuring the device ..............................................................................13 Setting the device location ...................................................................15Setting up the
thisonly after the pairing is completed. Setting the device locationUsing the Wiser Home app, you can assign the Relay in the room (such asbedroom, living room, dining room etc.).To assign the Relay location: 1. On the Home screen, tap . Device Details OPTIONS ABOUT Fil Pilote Delete ? AB DUG_ELKO
can test the Devices. To configure a Device: Choose the Device type (Light and Shutter Devices). Choose the specific Device type, e.g. rotary dimmer. Connect the Device to the app by setting it into pairing mode. The app will show you how to set the Device into pairing mode. Set the Name for the Device. Assign the Device to a Room. Test the Device.
........................................................13Configuring the device ..............................................................................16 Setting the device location ...................................................................18Setting up the LED Indicator Behaviour
Elko Wiser Home – Brukerveiledning for systemet (Norge)
Innstilling av tariff . Systemet administrerer strømpriser med en nøyaktighet på 0,01 €/kWh. Eksempel: Den gjennomsnittlige strømprisen per dag er 0,24 €/kW. Du har oppgitt at automatiseringen skal utløses når den daglige gjennomsnittlige strømprisen faller under 0,24 €/kWh. Prisoppdatering 1: 0,235
..............................................................................22 Setting the device location ...................................................................24Setting Dimming Mode ........................................................................24Setting up the Power On Behaviour
elko.no/contact www.se.com Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Selecting the operating mode