Showing 51 - 60 of 272 results

Page 6 of 28
  • ELKO - SmartMove Relay 10A Wiser Home Device user guide

    not be visible if you have only a single devicein the Wiser System. All functions will be accessible through the Homescreen. Away ModeAway Mode automatically turns off the Motion Sensor Switch. For example, whenyou are away from home for a long time, the light should not turn on due to falsemotion
  • ELKO - SmartMove Multiwire Dimmer Push Wiser Home Device user guide

    - SmartMove Multiwire Dimmer Push 2. On the Device Control Screen, drag the slider bar up/down to increase/decrease the brightness (A). TIP: You can also turn on/off the device on the Device Control Screen, tap (B) to turn on/off the Motion Sensor Dimmer. Away ModeAway Mode automatically turns off the Motion
  • Elko Wiser Home System User Guide (Norway)

    devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay safe and simulate your presencewith lights and shutters when you areaway for added security Show me Not for me ShutterLiving room Openuntil 16:00 Automations 60 SUG_NO_WH-01
  • Wiser Home AI

    Elko Wiser Home – System User Guide (Norway)

    or deactivate loads. Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions. Supported
  • Bortemodus

    ELKO - SmartPir m bryter 10A – Brukerveiledning for Wiser hjem-enhet

  • Bortemodus

    ELKO - SmartPir med dimmer – Brukerveiledning for Wiser hjem-enhet

  • Bortemodus

    ELKO - SmartPir Dim Multi Wire – Brukerveiledning for Wiser hjem-enhet

  • ELKO - Smart Plug 16 A Wiser Home Device User Guide

    A 24 DUG_SmartPlug 16A_ELKO_WH-00 ELKO - Smart Plug 16 A 4. Tap Add conditions and select any of the following (C): – Device status change: To select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off
  • Bortemodus

    Elko Wiser Home – Brukerveiledning for systemet (Norge)

  • Creating an automation

    ELKO - Smart Water Heater Puck – Wiser Home Device User Guide

    condition must be met to trigger an automation. Tap Add conditions (C) and select any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Energy Price changes(To define the energy price limit) This condition is available only if your tariff is set to Peak/Off-Peak
Page 6 of 28