Showing 71 - 80 of 80 results

Page 8 of 8
  • Pairing the main device with On Grid solar system

    ELKO Smart Tag – Wiser Home Device User Guide

    help to prevent power tripping by shutting down loads in order to keep the power consumption under a defined limit. By default, the grid limit is set to measure in kVA. Select your grid limit (kVA/A/kW) from the dropdown menu, then tap and enter a value using the dial pad as per your country. The
  • Account settings

    Elko Wiser Home – System User Guide (Norway)

    Home, Apple Home, and Amazon Alexa, ensuring seamless interaction between your smart devices. Refer to Matter for details information. Privacy Management Activate or deactivate the option to receive marketing emails and contribute to data analysis for service improvement. It also provides information
  • Seasonal Comfort Mode

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    home’s geographical location. It manages the shutters dynamically based on the real-time temperature conditions to improve comfort. Advanced Level - Best-in-class optimization with light sensors: At this level, it further improves the shutter management by using the real-time light intensity measured
  • Seasonal Comfort Mode

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    home’s geographical location. It manages the shutters dynamically based on the real-time temperature conditions to improve comfort. Advanced Level - Best-in-class optimization with light sensors: At this level, it further improves the shutter management by using the real-time light intensity measured
  • Seasonal Comfort Mode

    Elko Wiser Home – System User Guide (Norway)

    conditions to improve comfort. Advanced Level - Best-in-class optimization with light sensors/outdoor motion sensors: At this level, it further improves the shutter management by using the real-time light intensity measured by the outdoor motion sensors and the indoor and outdoor temperature. Make
  • About the document

    ELKO Smart Tag – Wiser Home Device User Guide

    including grid, solar, and battery systems. The document also covers device management tasks such as renaming, identifying, and removing devices, as well as setting up automations and notifications. Validity Note The characteristics of the products described in this document are intended to match the
  • ELKO Smart Tag Wiser Home Device User Guide

    yourcontract. It will help to prevent power tripping by shutting down loads inorder to keep the power consumption under a defined limit. By default, thegrid limit is set to measure in kVA. Select your grid limit (kVA/A/kW) from the dropdown menu, then tap andenter a value using the dial pad as per your
  • ELKO - SmartDim Multiwire Universal LED Rotary Wiser Home Device user guide

    manually turn on/off the dimmer and increase/decrease brightness level.This will provide power to the load connected to it.Short press the push button (< 0,5 s) once to switch on/off the dimmer. To increase brightness, turn the dimmer knob clockwise, and to decreasebrightness, turn it anti-clockwise. 25
  • ELKO - SmartBlinds Puck Wiser Home Device user guide

    . • Advanced Level - Best-in-class optimization with light sensors:At this level, it further improves the shutter management by using the real-time light intensity measured by the outdoor motion sensors and the indoorand outdoor temperature.It offers maximum efficiency by adapting shutter movements based on
  • ELKO - SmartBlinds Push Wiser Home Device user guide

    shutter management by using the real-time light intensity measured by the outdoor motion sensors and the indoorand outdoor temperature.It offers maximum efficiency by adapting shutter movements based on actualtemperature and natural light, rather than relying only on the estimatedsunrise/sunset times. TIP
Page 8 of 8