Showing 81 - 90 of 272 results

Page 9 of 28
  • Seasonal Comfort Mode

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Seasonal Comfort Mode Seasonal Comfort Mode Seasonal Comfort Mode The seasonal comfort mode uses the predicted temperature of a location or information from the light and temperature sensors to determine the temperature of a room and maintain a desired temperature in it by opening or closing the
  • ELKO - Wiser Room Thermostat Wiser Home Device user guide

    Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information about AwayMode, refer to the system user guide. 5. Tap Device status change > . Set the temperature using sliding bar (D
  • ELKO - SmartSensor Leakage Wireless Wiser Home Device user guide

    triggers an action only when all conditions are met.– Any condition: This triggers an action when at least one condition is met. 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an
  • Elko Wiser Home

    Deleting a Schedule Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Modes Modes Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison
  • ELKO - SmartDim Multiwire Universal LED Rotary Wiser Home Device user guide

    the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in
  • ELKO - SmartMove Multiwire Dimmer Push

    Rueil Malmaison France elko.no/contact www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue
  • Troubleshooting in Quick Home Connect

    ELKO - SmartDim Multiwire Universal LED Push – Wiser Home Device user guide

    -button dimmer Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing Pair the device again. Refer to Push-button dimmer The Wireless switch
  • Troubleshooting in Quick Home Connect

    ELKO - SmartSwitch Push 10A – Wiser Home Device user guide

    SmartSwitch push Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing Pair the device again. Refer to SmartSwitch push The Wireless switch
  • Troubleshooting in Quick Home Connect

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Control Switches Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing Pair the device again. Refer to Blind Control Switches The
  • ELKO - SmartSwitch Push 10A Wiser Home Device user guide

    select any of the following (C): – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On
Page 9 of 28