ESXP2GE013EN-05

With Connected Products and Remote Services

In this architecture, the data is collected and recorded from all connected products using a cloud gateway (EcoStruxure Panel Server). It is then passed on to the EcoStruxure Asset Advisor platform and interpreted by experts as part of the EcoStruxure Service Plan.

The recommended digital architecture for the application is shown below:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?