ESXP2GE013EN-05

Outputs

Display of the following outputs is performed by EcoStruxure Power Monitoring Expert, Power Operation, or via the Asset Advisor web platform.

Live Data Display

Live diagnostics data from monitored equipment can be visualized if the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) is in the architecture.

Events and Alarms

Asset related events and alarms can be raised in EcoStruxure Power Monitoring Expert and/or Power Operation in real time, or near real time, depending on the system configuration. These include MV switchgear and transformer environmental conditions (temperature and humidity), busway junction temperatures, breaker health (aging) and other simple diagnostics (communications, status, etc.).

Reports

Reporting is available for asset health analysis with Edge Control Software (EcoStruxure Power Monitoring Expert and Power Operation).

It includes:

Low Voltage Circuit Breaker Aging Report *

The circuit breaker aging report shows the status of circuit breaker aging and wear in your electrical system. The following LV circuit breaker ranges are supported:

  • MasterPacT MTZ 1/2/3

  • MasterPacT NT

  • MasterPacT NW

  • ComPacT NS630b-3200

  • PowerPacT H-, J-, and D-Frame (China)

UPS and Generator Battery Health *

Reporting for assets such as generators, generator batteries, and UPSs can be found in the Backup Power Testing Application section.

Notifications *

There are various options for remote notifications depending on the selected architecture:

  • Simple diagnostic notifications based on data from supported connected products in the Edge Control software (Schneider Electric circuit breakers, protection relays, UPS, etc.)

  • Preventive maintenance notifications based on EcoStruxure Asset Advisor Preventive analytics for Schneider Electric MV/LV equipment

  • Proactive/Predictive analytics alerts and recommendations with EcoStruxure Asset Advisor Predictive for Schneider Electric MV/LV equipment and third-party equipment

Cloud-Based Analytics and Services

EcoStruxure Service Plan powered by EcoStruxure Asset Advisor provides remote monitoring, asset management consulting, and on-site maintenance activities with recommendations from our Schneider Electric service experts.

It includes:

  • Continuous asset monitoring and alarms

  • Web portal and mobile app consultation with 24/7 remote support

  • Remote notifications in the event of electrical asset condition anomalies

  • Predictive analytics to help determine remaining equipment lifetime and other health indicators

  • Customized reports with recommendations on asset health condition and optimized maintenance plan

  • Condition-based asset maintenance triggered by Maintenance Index

  • Optimized maintenance plan and proactive recommendations from Schneider Electric experts

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.