DOCA0151EN-11

Firmware Version 8.0.37

New Features

Integrated BSCM Modbus SL/ULP module with FDM128.

Bugs Fixed

  • FDM128 was not able to discover PAS400.

  • Auto-discovery is not happening properly via PAS600 or PAS800.

  • FDM128 raises false high priority alarm dialog box during the MasterPacT MTZ circuit breaker boot up.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?