FDM128 Ethernet Display For Eight Devices
The FDM128 Ethernet display for eight devices (LV434128) is a 1-to-8 human machine interface (HMI). The main component is a 5.7-inch touchscreen.
An FDM128 display can be connected to devices via an Ethernet interface by using any of the following options:
-
One or more Ethernet gateways (IFE server, Link150, PowerLogic EGX300 and EGX100, PowerTag Link, PowerTag Link B, PowerTag Link HD, Smartlink SI B, or Smartlink Ethernet).
-
One or more third-party Ethernet gateways that possess the appropriate characteristics.
The FDM128 display monitors and controls up to eight devices from the following list:
-
Circuit breakers equipped with communicating MicroLogic trip units, such as:
-
MasterPacT MTZ circuit breakers
-
MasterPacT NT/NW circuit breakers
-
ComPacT NS circuit breakers
-
PowerPacT P- and R-frame circuit breakers
-
ComPacT NSX circuit breakers
-
PowerPacT H-, J-, and L-frame circuit breakers
NOTE:-
The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers in this guide applies to the existing range ComPacT NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.
-
The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this guide applies to the existing range ComPacT NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.
-
These new ranges are based on the same technical and dimensional architecture as that of the exiting range of circuit breakers.
-
-
Switch-disconnectors, such as:
-
MasterPacT NT HA switch-disconnectors
-
MasterPacT NW NA/HA/HA10/HF switch-disconnectors
-
ComPacT NS NA switch-disconnectors
-
ComPacT NSX NA switch-disconnectors
-
PowerPacT P- and R-frame switch-disconnectors
-
PowerPacT H-, J-, and L-frame switch-disconnectors
-
-
PowerTag Link devices, such as:
-
PowerTag Link gateway
-
PowerTag Link B gateway
-
PowerTag Link HD gateway
-
-
Smartlink devices, such as:
-
Smartlink SI B gateway
-
Smartlink Modbus gateway
-
-
EcoStruxure Panel Server devices, such as:
-
EcoStruxure Panel Server Universal
-
EcoStruxure Panel Server Advanced
-
EcoStruxure Panel Server Entry
-
The information displayed includes measures, alarms, and operating assistance data.