DOCA0151EN-11

Firmware Version 8.0.25

New Features

  • Integrated the new devices: ComPacT NS and PowerPacT P- and R-frame circuit breakers. These new ranges are the evolution of existing ComPact NS and PowerPact P- and R-frame range of circuit breakers.

  • Added new screens to display power and energy readings for the following devices:

    • PowerTag F160 energy sensor (A9MEM1580)

    • PowerTag Rope energy sensors (A9MEM1590, A9MEM1591, A9MEM1592, and A9MEM1593)

    • PowerTag M250/M630 energy sensors (LV434020, LV434021, LV434022, and LV434023)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?